cancel
Showing results for 
Search instead for 
Did you mean: 

Antenna selection and layout for the Teseo-Liv3r GPS

NataliaNPL
Visitor

Hello everyone!

I'm a beginner in hardware design and I'm trying to design a simple smartwatch. For the GPS function I decided to use the Teseo-Liv3r. The fact is that in the user manual they indicate several types of antenna, in this case I have selected one of the recommended ones, the ANT1818B00BT1516S.

My questions are:
+ Section 8 is the recommended layout, it tells me to use a 50 ohm line, how can I calculate the track thickness correctly?
+ On the other hand, section 9.1.2 shows an example layout, does it maintain a specific distance between tracks?
+ I understand that surrounding the track path is to ensure the RF path, should I take into account that tracks pass under the path in other layers? Or, if there is a ground plane, would it not affect it?

Finally, do you think I should use another type of antenna for my design? I'm looking for something small, but I'm not sure which one to choose.

Thank you very much in advance

1 REPLY 1
GalaxyQuest
ST Employee

Hi Natalia,

I have forwarded your question to our EMEA marketing and apps. I am not very knowledgeable in RF side, so would like our h/w engineer to guide you.

Since this is holiday break next week, please expect a delay in response. Apologize for the inconvenience.

Thanks,

George.

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.