Subject | Author | Posted | |
---|---|---|---|
The current script in BlueSTSDK examples (https://github.com/STMicroelectronics/BlueSTSDK_Python) n...
| 2022-03-16 09:57 AM | ||
Hi! I have sensortile.box. I want to capture (lsm6dsox)mlc data for unico gui. I followed the steps...
| 2022-02-21 10:27 PM | ||
In this for the i2c communication I am planning to use LSM303DLHC for undersatnding the i2c communi...
| 2022-02-09 01:54 AM | ||
2022-01-22 04:04 PM | |||
Hello, I bought the STEVAL-STWINKT1B development kit and I used the High Speed Datalog example a...
| 2022-01-14 08:58 AM | ||
For the motionAD library, how are the three sensor data (accelerometer, pressure, temperature) used...
| 2022-01-09 11:21 PM | ||
2021-11-26 09:37 AM | |||
ADC Sampling rate :- Total Conversion Time (Tconv) = Samplingtime + 12 (This 12 is for 12-bit reso...
| 2021-11-23 08:05 AM | ||
I would like to be able to use FW OTA with AlgoBuilds. Any direction you can provide would be gre...
| 2021-04-20 10:08 AM | ||
Hello Friend i have a problem about vl53l0x measurement sensor. i send a error message while open t...
| 2020-12-30 04:48 AM | ||
the possibilies are: • VL53LX_DISTANCE_SHORT • VL53LX_DISTANCE_MEDIUM • VL53LX_DISTANCE_LONG ...
| 2020-12-03 08:28 AM | ||
Hey guys, I am currently trying to interface a VL6180x to a micro controller and when i try read...
| 2020-12-02 01:29 AM | ||
API Status: -6 : Range error =============================== //my code ..... if(Status == ...
| 2020-11-23 01:03 AM | ||
Hi ST Micro, I have tested the X-CUBE-53L1A2 software with X-NUCLEO-53L1A2 expansion board, I c...
| 2020-11-15 07:12 PM | ||
2020-10-29 03:34 AM | |||
I am on my second X-NUCLEO-53L0A1 board, a replacement for the first board that suffered from the s...
| 2020-10-07 08:37 AM | ||
I am using ISM330DLC accelerometer, the FIFO mode is Bypass-to-Continuous and the trigger is WAKE_U...
| 2020-09-28 01:31 AM | ||
I'm using the STEVAL-MKI109v3 demo board with the STEVAL-MKI193 IMU. I'd like to evaluate use of t...
| 2020-09-04 12:51 PM | ||
Hello, I am writing this message to you because I need help, if it is possible I would be grateful ...
| 2020-07-23 07:31 AM | ||
2020-07-20 10:30 PM |