Subject | Author | Posted | |
---|---|---|---|
2020-06-01 6:55 PM | |||
2020-05-26 11:27 PM | |||
I am using the STM32F769II processor, I am communicating with the display in RGB565 mode using LTDC...
| 2020-05-21 6:56 AM | ||
2020-05-20 5:21 AM | |||
Hi, I'm working on a Window that contains a Listbox and some buttons. When I touch Listbox's area,...
| 2020-05-17 9:58 PM | ||
2020-05-17 4:19 AM | |||
I'm thinking about using a high resolution display like this one https://www.ebay.com/itm/1133...
| 2020-05-14 10:29 PM | ||
As far as i understood the DCMI on AHB2 bus which has speed of (CPU/2 ) so at 480 MHz it will be 24...
| 2020-05-14 1:01 AM | ||
This question was asked before 5 or 6 times but no meaningful answer was provided. How to use B-LC...
| 2020-05-08 2:33 AM | ||
Hi: I used stm32cubemx to generate the LCD program,Use the FSMC driver.Ram space is limited, so use...
| 2020-05-07 1:06 AM | ||
Using the above parts, I am making a camera module to only take snapshots. I am using a 2MP sensor ...
| 2020-05-04 7:31 AM | ||
I found that PIXCLK must be always available in DCMI JPEG mode, then DCMI interface would detect V...
| 2020-05-03 5:18 PM | ||
I programmed DCMI interface, and I can see the VSYNC, HSYNC waveform on the pin of STM32L496, but ...
| 2020-04-29 7:59 AM | ||
Hi, my name is João. I'm graduated in Electronics Engineering from Federal University of Santa ...
| 2020-04-29 6:13 AM | ||
I have a FHD 1920x1080 touchscreen panel that has a 40pin eDP connector. Can any of the STM series...
| 2020-04-27 2:29 PM | ||
Hello, I am writing to you because I need help to solve my problem. Here is the situation: I am ...
| 2020-04-19 7:34 AM | ||
Hello everyone Does anybody know how do I change the text direction in STemWin library? I mean I w...
| 2020-04-17 1:09 AM | ||
Hello, I try to figured out if STemWin use the DMA2D to display JPEG or BMP when configured in 2...
| 2020-04-16 8:47 AM | ||
Hi I'm new to STM32. I need to capture data from ADC with high frequency. if I capture data durin...
| 2020-04-15 8:29 AM | ||
Hi I jist bought a STM32F469NI-Discovery board recently and I am unable to make the display work. ...
| 2020-04-14 1:41 PM |