cancel
Showing results for 
Search instead for 
Did you mean: 

Can I drive a 4-lane mipi display with a STM32H7?

m4l490n
Senior

I'm thinking about using a high resolution display like this one

​https://www.ebay.com/itm/113385033095

But​ I read in the STM32H7 reference manual that it only has two mipi lanes, so my questionis if it is possible to drive a 4-lane display with only 2 lanes, and if possible what would be the impact.

Also​, is there a 720x1280 5.5", 6", 7", or 8" display with only two mipi lanes?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0