Subject | Author | Posted | |
---|---|---|---|
Hello I am using ST7735 TFT display with STM32l4. All the spi configuration is correct. I am ab...
| 2020-12-30 04:13 AM | ||
Decoded VGA size JPEG images on STM32H750B-DK. As a result of measuring the decoding processing ti...
| 2020-12-21 04:12 PM | ||
Dear TouchGFX team, I am developing STM32L4R9 B/D including DSI video mode LCD, PSRAM, Oct...
| 2020-12-17 08:05 PM | ||
Is there some help to build project group with library and spread touchGFX code in different librar...
| 2020-12-15 10:59 AM | ||
Hi, We have created a custom PCB for our project using STM32L4R9ZI. We are using 390*390 AUO Di...
| 2020-12-11 04:03 AM | ||
Q&A session from webinar "Low cost GUI solution with TouchGFX" 2. TouchGFX looks impressive conc...
| 2020-12-11 04:02 AM | ||
Hello, I'm developing a HAL-based software running on STM32F778AI MCU. The software uses the hardw...
| 2020-12-09 12:53 PM | ||
Hi everyone, I am taking part in a project about display and controller using TFT AT070TN92 with g...
| 2020-12-03 07:19 PM | ||
Hi I do have a resitive touch xpt2046 and a ssd1963 screen. All widgets work fine except the ...
| 2020-12-03 09:24 AM | ||
2020-12-02 12:28 AM | |||
Hi, I want to write a text from keyboard widget on touchgfx but i do not this only on keyboard, als...
| 2020-12-01 05:58 AM | ||
I have connected LTDC output to VGA monitor input and the picture is flickering. I've connected HSY...
| 2020-11-30 04:28 AM | ||
Hello, I am trying to display something on the display of a STM32F413ZH board. Following the vid...
| 2020-11-30 01:20 AM | ||
My result for use CubeIDE versions is strange. Every version have deep troubles. One my project i ...
| 2020-11-27 06:54 AM | ||
I see the office usage as follows //read the binary font from a file
FILE* font = fopen("generate...
| 2020-11-26 06:10 PM | ||
Hi ST Community, I have a project started in keil, configured through CubeMX via keil's "Manage...
| 2020-11-26 07:26 AM | ||
I am trying to setup this LCD controller to drive a custom segment display, 22 segments, two backpl...
| 2020-11-24 07:45 AM | ||
Multiple selection of rows are intended or it is a side effect? Why if i set the same functionali...
| 2020-11-23 11:50 PM | ||
Hello everybody Does anyone set up USB camera?
| 2020-11-22 01:24 AM | ||
2020-11-17 12:01 PM |