Subject | Author | Posted | |
---|---|---|---|
2020-11-17 12:01 PM | |||
Hello, Still developping on my STM32H753VT6 with touchGFX. Instead of loading images with touchG...
| 2020-11-17 07:30 AM | ||
The picture is a snapshot to show the files imported (by the IDE) when the project was created. I'd...
| 2020-11-15 07:03 AM | ||
Hi team, I am using touchGFX in project, I would like to know how can I add user defined files or f...
| 2020-11-12 06:39 AM | ||
Hi there! I recently get the STM32H745 Discovery board and am trying to get it working with the LT...
| 2020-11-12 01:49 AM | ||
Hello I am using an STM32H743 MCU that implements acquisition of frame from camera and compres...
| 2020-11-11 12:24 PM | ||
Hi I am using H753 with its LTDC as display output. Due to a special request, H753 must know whe...
| 2020-11-11 09:33 AM | ||
Hello, I'm using STM32H745I with STMCubeIDE with STemwin and OPENAMP. Both core are active and ru...
| 2020-11-11 04:08 AM | ||
Hello, I'm trying to interface STM32H745I Custom board device with 800x480 Pixels 24bit TFT usin...
| 2020-11-06 04:10 AM | ||
Hi stm, We are working with 240x320 resolution display by the following configuration 1 d...
| 2020-11-05 07:26 AM | ||
Hello. I'm trying to create custom container with any number of elements. I created custom contai...
| 2020-10-28 04:52 AM | ||
Hi folks, I am trying to create a simple GUI with the BSP library on a STM32H747-Discovery boar...
| 2020-10-27 08:12 AM | ||
I have created an array of flex buttons in my user code for which I set attributes like text and bo...
| 2020-10-26 05:20 AM | ||
2020-10-23 01:16 PM | |||
I have a lot of TextAreaWithOneWildcard objects on screens, and more recently started using them in...
| 2020-10-15 01:09 PM | ||
I have saved a bitmap-file at 0xC0000000 external SD-RAM. How can I display this photo with TouchGF...
| 2020-10-15 02:08 AM | ||
Does on-chip RAM have to be contiguous when using LTDC functionality? Can the RAM address be change...
| 2020-10-09 02:49 PM | ||
I can't figure this out, I know how to set the different blink modes: LCD_BLINKMODE_SEG0_COM0, (B...
| 2020-10-07 12:32 AM | ||
Hi, I have an application that needs to print to a thermal panel printer. This would include ...
| 2020-10-05 09:04 AM | ||
Dear all, I'm developing an application with a STM32750N8 and I'm using TouchGFX for the GUI. ...
| 2020-10-05 01:07 AM |