User Activity

Hey There,I am working on a project that will involve using a STM32H743VIT6. Its quite a complex board so almost all of the pins one the MCU have been occupied. Because of this I have to drive the 240x320 LCD-TFT with SPI ( Driver is ILI9341). I was ...
Hey There,I am working on a project that will involve using a STM32H743VIT6. Its quite a complex board so almost all of the pins one the MCU have been occupied. Because of this I have to drive the 240x320 LCD-TFT with SPI ( Driver is ILI9341). I was...