Subject | Author | Posted | |
---|---|---|---|
ST8024CDR I have problem for reset smart card after smart card return (ATR) can received 1 byte is...
| 2023-05-30 10:35 PM | ||
I'm trying to program some data into a flash sector but the HAL_FLASH_PROGRAM returns a value of 1...
| 2023-05-30 8:32 AM | ||
Header file: /**
* @file I2CCommunication.h
* @brief Header file for controlling I2C message...
| 2023-05-30 5:54 AM | ||
Hello, I have successfully setup ADC3 to measure values on channels PC2_C, PC3_C, temperature, ....
| 2023-05-30 3:56 AM | ||
Good day. I wanted to know why the MotionAC library is not supported on the STM32L073 MCU. And is ...
| 2023-05-29 11:57 PM | ||
I'm setting up a new computer. I tried to download STM32 installer for windows 11 from this page ht...
| 2023-05-29 5:13 PM | ||
In my project, I'm using the STM32L476RELQFP64 microcontroller to process data from an external ADC...
| 2023-05-29 5:20 AM | ||
Could you please provide guidance on how to flash the firmware and configure the system to boot fro...
| 2023-05-29 3:30 AM | ||
Hello St community, I wanted to know if STM32U575I-EV example SMARTCARD_ComDMA support both T = ...
| 2023-05-28 11:14 PM | ||
I'm working on a project using an stm32f411 and somehow the halfduplex spi only return's once witho...
| 2023-05-28 9:41 AM | ||
I have a application with STM32F429ZI and SD card withour RTOS. I have a llong time for write in a...
| 2023-05-26 5:14 AM | ||
Hello everyone, I'm using stm32f103 with bluenrg-m2 over spi on custom hardware, I can send and re...
| 2023-05-26 3:53 AM | ||
It doesn't work even when I manually do the build just before launching. It doesn't work properly ...
| 2023-05-26 1:08 AM | ||
Hi Team, Here is what I'm expecting (this is only to reduce application size during FOTA): To p...
| 2023-05-25 11:02 PM | ||
First apologies in advance if I'm posting to the wrong place as I couldn't find any "post to" for S...
| 2023-05-25 4:39 PM | ||
void Comp1Init(void) { Comp1GpioInit(); RCC -> APB2ENR |= 1; //20230506 ////////////////////...
| 2023-05-24 1:51 AM | ||
Hello! I am a beginner and I am trying to implement a simple I2C communication with the DAC AD5675...
| 2023-05-23 4:53 AM | ||
2023-05-18 3:42 AM | |||
Hello, I succefully figured out to scan ADC1 and ADC2 (countinous mode) with DMA. The issue is tha...
| 2023-05-18 2:09 AM | ||
2023-05-17 11:25 PM |