User Activity

Please help i need to know about. Smart card interface ST8024CDR it can support Smart card ISO7816-3 in reset mode synchronous or not ? Now i using this ic it support only asynchonously asynchonously reset timming diagramsynchonously reset timming d...
ST8024CDRI have problem for reset smart card after smart card return (ATR) can received 1 byte is 0x3BParameterOSC = 4MHzCLKDDIV = 4Card is type T0 and support Max speed 5MHz Code start resetHAL_GPIO_WritePin(RST_UC_GPIO_Port, RST_UC_Pin, GPIO_PIN_SE...