Hi, please can someone help me? when I try to deploy I get the following error: PayloadTooLargeError: request entity too large at readStream (C:\Users\diego.mavillonio\AppData\Local\STM32CubeMonit...
I've started using the recently published UM3291 to have smoother workflows with my other acquisition tools There are a few glitches that makes life a little bit more annoying than it should...
Trying to monitor a 'C' variable of type bool results in the error not connected ! bad parameter (7) and the probe connection drops. It then comes back all on its own!! Changing the variable to ...
Please refer to screen shot cube Monitor overall. It all works except that the text does not display. I am expecting the numerical data displayed on the gauge would also be displayed in the Text on t...
Hi, I use CubeMonitor V1.8.0 with my STM32G474QET device. Unfortunately the chart inside the dashboard is very small so I can`t work with it. Is there any possibility to set the size of the graph?...
I have followed this STM wiki tutorial about basic PD Sink. Everything is running according to it, but I am unable to see voltage and current measurement inside UCPD monitor. I have also followed the...
Hello, Today I tried using STM32CubeMonitor 1.7.0 on macOS Sonoma (MacBook with M1 chip), but after installing the app opens without acq in and acq out nodes in the library, and of course it co...
In the cube monitor I didn't have acquition in and acquition out nodes , how can I add these nodes to my pallette and send me the links to install these nodes to my pallette
Hello, I'm using a STM32G0B1RE and a nucleo SRC1M1 in order to charge and communicate with a tablet in power delivery mode with 5V 3A. I followed the following tutorial: STM32StepByStep:Getting ...
I need to start using STM32CubeMonitor on my NUCLEO-G071RB to monitor some variables of my new firmware application developed with STM32CubeIDE 1.15.0. I never used STM32CubeMonitor before, so I...