respected sir, i am using SPC560B54L5 and i am testing can protocol in pcan view i got error busheavy status . i am also checking on oscilloscope only getting rx signal from transceiver. CAN int...
Posted on August 08, 2017 at 08:29 Hello community, I am asking myself if there is actually anyone running FlexRay on the SPC56EL70L5 Board? I am currently stuck in the wakeup process (I...
I wanted to test Error Correction code (ECC) for the flash memory (for both data flash and code flash) and was looking out for a way to generate these error. In the Reference manual (SPC560P40L3 micr...
Hi, currently I am trying to realize the instructions of the guide which is included in the current download version 1.32 , but after executing erything eclipse showed me that there are...
Posted on March 06, 2017 at 21:26 Hello, Trying to make a workaround for the flash-not-ready-after-leaving-power-saving problem, I am placing the below function in a section which goes into th...
Hi, I would like to say if the FlexCAN inside the ST microcontroller SPC56EL70L5 supports the RX Individual Mask Registers (RXIMR). I read the CAN driver's implementation and it does not seem that t...
Posted on July 09, 2018 at 03:46 Hello I was told that the FPU is not normally enabled in the SPC5Studio (I am using the SPC56ELxx family), which is odd but ok. The issue is that I was told al...