2018-07-08 06:46 PM
Hello
I was told that the FPU is not normally enabled in the SPC5Studio (I am using the SPC56ELxx family), which is odd but ok. The issue is that I was told also that
through the build options in SPC studio it can be enabled. To save my life I cannot find this. Could someone help me.
Thanks!
C.
Solved! Go to Solution.
2018-07-10 09:01 AM
Hello Caio ,
did you compile with -mspe=yes ?
https://app-community.st.com/thread/43975-fpu-exceptions-on-spc56el60l3
Best regards
Erwan
2018-07-10 09:01 AM
Hello Caio ,
did you compile with -mspe=yes ?
https://app-community.st.com/thread/43975-fpu-exceptions-on-spc56el60l3
Best regards
Erwan
2018-07-11 08:57 AM
Thanks Erwan, it works!!
2018-07-11 10:59 AM
One detail: Is there a document or link where all these switches are defined?
Thanks!
C.
2018-07-11 11:00 AM
Hello Erwan
Thanks for the link, I set it and it is already working!
Best RegardsCaio D. Gubel(Cell) +1 (915) 355-5171
On Tue, Jul 10, 2018 at 9:01 AM Erwan Y <st-microelectronics@jiveon.com>