Hello everyone, I am currently working on programming the display of the STM32F469I-DISCO using X-Cube-TouchGFX. What I want to achieve: I aim to create a simple application that displays a button...
Hi all, as I'm new to TouchGFX I'm struggeling on a problem hat does not look difficult at first glance. My problem: On screen_1 there is a Text Area allowes the use to enter a string as input. T...
Hello! I set the wildcard range to 0x0000-0xFFFF to use all characters contained in the "Pretendard JP" font. However, I get an error when generating code with TouchGFX Designer. Of course...
Hello, I'm trying to setup a simple "Hello world" project for a custom board with an STM32H7A3IIT6. I've successfully created the project from CubeMX (6.12) generated the code for Keil MDK and, star...
Hi Currently we are developing a project based on the STM32H723. The project is a platform for different derivates. It uses as well Azure RTOS. We used STM32CubeMX to generate reference code. Bu...
Hello. I would use a static graph to display data. In the handletickevent function, I update the addDataPoint(x data, y data) function for the given page, but nothing appears on the graph, the scale...
I have just upgraded my project from TouchGfx 4.22 and on rebuild I get: (.text._ZN8touchgfx8LCD16bpp19DecompressorRGB_QOI16blitCopyARGB8888EPKhRKNS_4RectES6_h+0x31c): undefined reference...
Hello! Our project is supposed to use C++17 features. When linking C++17 compiled objects against TouchGFX Designer's distributed binaries (eg: touchgfx_core.a), linkage fails, because the tou...
Hi everybody, I'm trying to implement into a custom board, the dynamic Qrcode generation algorithm. I'm using touchgfx 4.23.0, an SPI display with partial buffer strategy. I would like to draw the...
Hi, I have used TouchGFX on an F4 without any problems so far, except that the animations were a bit slow. Now I bought this H7A3ZIQ and when I add TouchGFX to the project, I get 230 'undefined refe...