Hello, I am trying to make my own custom USB PD application on NucleoG0B1RE + SNK1M1 hardware. I want to change dynamically the SNK PDOs in my application (it should be possible according to this p...
Hello,
I have a setup where I use an STM32H747XIH6U and an ADAU1361 codec on the I2S-interface. I want to use the PDM-mics on the ADAU, and in order to do that, ADAU has to be in I2S master mode ac...
Hello, I want to use X CUBE USB AUDIO examples in X CUBE IDE. After generating the binary code (without errors) and flashing the binary code via DFU, the card is not recognized as an audio ...
I am using the NUCLEO-G474RE along with the X-NUCLEO-SRC1M1 board to create a USB-C power delivery source. I am also using the "SRC1M1_Source" example project in the x-cube-tcpp software downloa...
I using OLED I2C display and its interface with STm32F091VBT6 MCU. My application is fuel dispensing i face issue while dispensing the OLED display is stuck. i cant find any error. can any body know ...
Dear Sir/Madam, Is it possible to have a STM32 with build in UCPD-controller to deliver 240W at the port? or does anyone have experience with this type of application? According to (link: ht...
I do not know if this is appropriate place to ask but I will try. We are integrating the STM STL library and we cannot get the flash test to be successful. This, this, this nor t...
Hello, Please excuse the basic question, I am reading the datasheet of stm32f429ve trying to understand which pins I need to send data from the microcontroller to an audio codec using I2S....