cancel
Showing results for 
Search instead for 
Did you mean: 

Visual glitch for file attachments

Piranha
Chief II

When a link is given to a particular post and the post has a file attached, two horizontal lines appear under the small file icon.

https://community.st.com/t5/stm32-mcus-products/stm32f4-hardfault/m-p/604656/highlight/true#M226598

Piranha_0-1699131558158.png

As can be seen in the picture, the lines do not appear on other posts with file attachments. And, if one takes a link to the second post of the two, then the lines appear on the second post but not on the first one.

3 REPLIES 3
Lina_DABASINSKAITE
Community manager
Community manager

Hello @Piranha , 

Good catch! I can replicate this as well. Passing this for further investigation. 

Thanks,
Lina

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Piranha
Chief II

A somewhat related issue. When hoovering over the file attachment paperclip icon, the mouse cursor turns into a "finger", which is normally used for URLs. As there is no actual URL attached to it and clicking on the icon does nothing, the cursor over it should not be a "finger" type, which definitely signals that some action will be done. Also the same happens while hoovering over the file names of archives and other attachment file types, which doesn't have a preview functionality.

Here is an example with a RAR file:

https://community.st.com/t5/stm32-mcus-products/hal-delay-not-working/m-p/75032/highlight/true#M7727

Also one can see the same behavior for the following file types in ST's testing environment.

ICO, FLV: https://qa-stcommunity.st.com/t5/analog-and-audio/attachments/td-p/366

TAR, ZIP, 7Z, RM, RAR: https://qa-stcommunity.st.com/t5/power-management/attachments-2/td-p/368

Hi @Piranha ,

Thanks for your feedback, we are investigating this issue as well.

Michael