2026-02-24 3:44 AM
For the past week or so, pasting images directly into posts seems to have broken.
I used to be able to just take a screenshot, or copy an image and paste it straight into the editor, but that no longer works.
I press 'paste', and nothing happens - no error messages or anything.
I am now having to save the image locally, and then use the 'Insert Photos' button to import it.
There is history with this, but now it seems to have just broken completely.
Using Chrome Version 145.0.7632.109 (Official Build) (64-bit) on Windows-11 Pro
Solved! Go to Solution.
2026-03-04 7:19 AM
I'm actually referring to the other bug. Maybe it's best in a new thread.
2026-03-13 3:26 AM
@Maxime_MARCHETTO1 @Lina_DABASINSKAITE It's still not working, but the behaviour has changed.
I just tried to paste am image; it still didn't work, but I did get an error this time:
https://community.st.com/t5/others-stm32-mcus-related/usb-c-pd-analyzer-tool-used-in-an5225/m-p/885682/highlight/true#M9688 - I subsequently posted the image by saving to file, then using drag & drop into the post
2026-03-13 4:13 AM - edited 2026-03-13 4:14 AM
Thanks @Andrew Neil. I passed this to the team. They are currently working on the fix. I will keep you posted once there are news. If you notice anything new, let us know.
Thanks!
2026-04-09 2:29 AM
Looks like it might be working again ... ?
2026-04-09 2:41 AM
Hi @Andrew Neil.
Yes, this has been fixed this morning as well. I am happy to see it's working for you!
Lina