2024-12-12 02:36 PM - last edited on 2024-12-12 11:40 PM by Peter BENSCH
This is what I see when writing a new message in the community (or creating a new post). Notice the </> option to insert code snippet.
However, en clicking on the `...` option to expand it, the </> is gone, and I can not find a way to collapse the options to what it was before.
It would be nice to have this fixed.
Many thanks.
Solved! Go to Solution.
2025-01-20 03:05 AM
Hello @eduardo_reis , all,
I confirm that this issue has been fixed and now editor works as expected.
Let know it everything works fine on your end.
Thanks,
Lina
2024-12-13 05:36 AM - edited 2024-12-13 05:52 AM
Hello @eduardo_reis
Thank you so much for reporting the issue. I can replicate this as well. I’m passing it to troubleshooting and will give an update once there’s news.
Let me know if there’s anything else,
Lina
2024-12-16 03:54 AM
Confirmed!
2024-12-16 12:27 PM
I assume it has been fixed recently? I see the </> symbol
2024-12-16 12:47 PM
Well it had been working for the longest time, so must have been "un-fixed" relatively recently.
Some of ST's posts, or "Knowledge" things, provide for different options wrt posting or answering against them.
I've definitely had to fish post-code or image out of the "..." options in recent weeks.
I've also seen the Emojis reappear during editing. Can we just remove these entirely, and act like grown adults?
2024-12-16 01:32 PM
Also seing the posts at the top-level not sorting based on newest posts, something has been fiddled with in the last week-or so.
2024-12-17 01:34 AM
2025-01-20 03:05 AM
Hello @eduardo_reis , all,
I confirm that this issue has been fixed and now editor works as expected.
Let know it everything works fine on your end.
Thanks,
Lina