2023-11-14
02:42 PM
- last edited on
2023-11-17
10:55 AM
by
Lina DABASINSKAITE
Incidentally, if Firefox browser Privacy and Security -> Do Not Track set to Always, then it is not possible to reply to posts here. Nor does the Accept as Solution option appear.
2023-11-14 03:44 PM
Thanks for the additional information about Firefox, we’ll check and try to fix it.
2023-11-17 10:59 AM
Hello @bWildered1 ,
First, let me welcome you to ST Community! I tried to replicate the behavior and could not replicate.
Could you share:
1. A screenshot of the outcome you get once the seating is set to "Always"?
2. Firefox version you use.
This would help a lot to investigate.
Thanks,
Lina
2023-11-24 02:32 AM
Hi Lina.
A little more, possibly useless, information that you can maybe stick into a memory somewhere in case it may be relevant in the future.
It may be possible that the problem was related to a failure to login, and that the Firefox settings were just a coincidence.
Occasionally I find it difficult to login to the ST site - largely due to poor Internet connectivity I suspect - and this replicates the same behaviour I reported, i.e.
1. There is no 'Accept as solution' option visible (probably because I am not logged in)
2. When 'Reply; is clicked, the system tries to load a new page - which I suspect is the logon page - but is unable to, displaying a blank page instead.
Sorry to have been so much trouble.
Take care.
M
2023-12-18 02:51 AM
Hello @bWildered1 ,
Thanks for this additional information. To answer your poits:
1. There is no 'Accept as solution' option visible (probably because I am not logged in)
LD: Yes, you are right. To be able to see accepted solution, create or kudo the post, you need to be logged it.
2. When 'Reply; is clicked, the system tries to load a new page - which I suspect is the logon page - but is unable to, displaying a blank page instead.
Yes, you are correct. You need to be logged in to type a reply.
As these issues is linked with the internet performance, I recommend get sorted that first.
Regards,
Lina