2024-02-27 2:34 AM
The forum sends emails like this:
It's good to remind people to mark the solution if there is one - but what if there isn't?
What if the answer to that question is, "NO." ?
See: Betteridge's law of headlines.
Perhaps the email should include some tips on what to do next - and what not to do next; eg, just "bumping" the post ?
2024-02-29 1:45 AM
Hi @Andrew Neil ,
Thanks for brining this up and suggesting an improvement.
Indeed, the system does not know if there is a potential solution or not. I agree, the email text could be improve and we'll consider the changes in the near future.
If anyone else, has additional suggestions, feel free to write them here!
Thanks a lot,
Lina
2024-02-29 1:59 AM
@Lina_DABASINSKAITE wrote:the system does not know if there is a potential solution
It does know when a 'Solution' has been marked - I think these messages are only sent for a thread that's been idle for a while, and with no 'Solution' marked?
2024-02-29 2:04 AM - edited 2024-02-29 2:59 AM
Yes, exactly. This is what I meant. Current rule is: the email is send after 7 days when there are questions with answers not accepted as solution.
2024-02-29 2:24 AM
@Andrew Neil wrote:Perhaps the email should include some tips on what to do next - and what not to do next; eg, just "bumping" the post ?
For example:
If the problem has not yet been solved, consider how you can help to move the discussion forward:
Just "bumping" the thread (making a post which adds no further information) is unlikely to help.
2024-03-13 3:54 AM
It seems to me that there are 5 scenarios: