2023-12-20 07:11 PM - edited 2023-12-20 07:13 PM
There are many threads where users have been unable to attach IOC files. Here is one of them:
https://community.st.com/t5/stm32-mcus-products/uart-cannot-set-high-baud-rate/m-p/621673#M230659
The IOC file type is clearly not a security concern. Is there some other reason they are blocked or is this just an oversight? Can we get it corrected?
Edit: I have no problems attaching an IOC file. So is this a permissions issue? New users can't attach files or something? I would say even a first time user first time poster here should be able to. Coming to a forum to ask for help and including the relevant file seems a very reasonable thing to do.
Cheers.
2023-12-20 07:35 PM
2023-12-22 01:51 AM
Hello @TDK ,
The IOC files are working and are allowed to use for everyone without any restrictions. We had some issues during the summertime with this file type, but they are sorted for some time. I will get it checked why this user faces issues.
@fkst tagging you here for visibility.
Thanks for highlighting this for us.
Regards,
Lina
2023-12-22 05:35 AM
Thanks @Lina DABASINSKAITE. Fairly sure this has come up at least a few times in the last 1-2 months so it's not a one-off thing, but I'm not going to go find the other threads--too hard to search. I'll post here again if I see that it happens again.
2023-12-27 06:08 AM
Hi @TDK ,
we performed tests and were unable to replicate this type of case.
Hi @fkst ,
could you download the file attached to the TDK post and try attaching it to a new post in this thread as a test? If you are unable to do this again, we would ask you to provide the following information:
It would allow us to investigate the issue for you and our community.
Best,
Adam
2023-12-27 06:46 AM
Well historically it has been an issue / complaint.
Users weren't able to attach an array of files, and we told them to rename .IOC with .TXT to allow attachment. Not sure it is case sensitive, or not.
Within the last week or two the attachment of .IOC seems to be permitted, at least to responses.
Perhaps double check for initial Top Posts (Question), or New Users, as these might have different rules / expectations, as to what is permissible.
#MandelaEffect
2024-01-10 11:57 PM - edited 2024-01-22 10:12 PM
Any update?
2024-01-11 04:11 AM
Hi @Tesla DeLorean ,
Thanks for the additional information. I just wanted to inform you that the tests you mentioned were carried out and were successful.
Best,
Adam
2024-01-11 04:14 AM
Hi @RogersKing ,
Are you currently experiencing issues attaching IOC files? If so, we would ask you to please provide the following information:
This will allow us to investigate the issue for you and our community.
Thanks,
Adam