Feedback forum

Raise questions or provide feedback on our community platform.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

st.com website

Good afternoon.I'm not sure this is the place to post this but here's the issue.  As of today, 9/13/2024, when I go to the st.com website I get an endless barrage of ST adverts that can't be stopped or bypassed.  I never get to the login panel, there...

TJM by Senior
  • 3368 Views
  • 10 replies
  • 0 kudos

Resolved! EMRT

I did not found the latest EMRT report. thanks!!!

KobE by Associate
  • 1309 Views
  • 2 replies
  • 0 kudos

Download of software fails again

Same symptom as already reported by so many people.After clicked thru all legalese stuff and logged in - downloads won't start.Instead there's the spinning thing, it just spins endlessly. No error messages. Browser: Edge on windows 11, all updated.Su...

PavelA_0-1726351532758.png PavelA_1-1726352107121.png
Pavel A. by Super User
  • 2989 Views
  • 10 replies
  • 6 kudos

Line numbers in source code blocks

It would be useful to be able to specify the starting line number in a source code block; eg, see:https://community.st.com/t5/stm32-mcus-products/how-to-use-stm32-lis3dh-driver/m-p/719871/highlight/true#M260772 (Yes, there are plenty of more pressing...

Missing option for strikethru text. Sometimes...

When editing a post, the strikethru (like this) style is missing. I clicked the area where the "..." should be to be sure there is no button. This is definitely a new bug. I could edit posts with strikethru before. Have noticed it a few times lately....

TDK_0-1724285601419.png TDK_1-1724285636430.png TDK_2-1724285699800.png
TDK by Super User
  • 2160 Views
  • 4 replies
  • 1 kudos

Zoom control for ALL attached images request

Example image without zoom controllRe: ThreadX thread and queue names not displayed p... - STMicroelectronics Communityexample with zoom controll i cant found now , but sometimes is showed bottom on image  and i mean this zoom control is required on ...

MM1_0-1717516867907.png
MM..1 by Chief III
  • 1710 Views
  • 5 replies
  • 1 kudos

Broken HTML in Notification title

 Doesn't happen in the thread itself: https://community.st.com/t5/stm32-mcus-embedded-software/stm32l4-hal-rtc-functions-do-not-check-hrtc-gt-instance-before/m-p/703427 

AndrewNeil_0-1722358675095.png AndrewNeil_1-1722358767743.png

multiple notifications for the same post

These two notifications refer to the exact same post:He couldn't have mentioned me without making a reply, so I really don't need two separate notifications!EDITAnd why are the two email notifications sent 7 minutes apart?! 

AndrewNeil_0-1707917580502.png AndrewNeil_0-1707917914560.png