cancel
Showing results for 
Search instead for 
Did you mean: 

Validation on target error

It is fine until validation on validation on desktop... but when it comes to validation on target, it is showing the above error...
can anyone please address my issue... I am trying this since 3 months..

22 REPLIES 22

Mam, still after including those pools, I am getting the same error...
What to do... Please solve...

I am sharing the screenshot with you

Could you please confirm that the compilation and flashing procedure performed correctly ?

Feel free to read this getting started for X-CUBE-AI: Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI) - User manual

 

Best regards,

Yanis

 

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

You mean debugging only right...??
In STM32 CubeIDE debugging is done without errors and warnings... While it is running, i opened the ioc file simultaneously and tried validation there in MX...

hamitiya
ST Employee

If you are debugging your current project, based on your IOC file, it means you are using SystemPerformance since it is the one generated by ST Edge AI Developer Cloud. "SystemPerformance" template generates inference output directly in UART which you can read on your COM port (with a tty such as putty)

If you want to validate on target, you need to do it automatically from X-CUBE-AI or generate a "Validation" template.

 

Best regards,

Yanis

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Please update me that process of validate on target... please
i need to do validate on target only....

On the documentation I shared before, page 15

I did it on my side here attached the ZIP corresponding to your project

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

May I please know what did you do in the above zip file mam.... so that i can do the same from next....

hamitiya
ST Employee

Hello,

I did exactly what I shared with you in my previous messages

​
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

If possible could you please help me through the process, I will give you remote access of my system...
It will be very helpful as many people are facing issue with validating on target...
I will provide the remote access so that you can show what to do...
Please update mam

mam please update... it is really urgent