un-understandable randomization of input data inside the generated code
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-02-26 2:22 AM
Hello,
I am using STM32CubeMX Ver 5.5.0 with X-CUBE-AI .
In the generated code inside function MX_X_CUBE_AI_Process() I found the following code just before aiRun function
/* ---------------------------------------- */
/* Data generation and Pre-Process */
/* ---------------------------------------- */
/* - fill the input buffer with random data */
for (ai_size i=0; i < AI_CNN_IN_1_SIZE; i++ ) {
/* Generate random data in the range [-1, 1] */
ai_float val = 2.0f * (ai_float)rand() / (ai_float)RAND_MAX - 1.0f;
/* Convert the data if necessary */
if (type_ == AI_BUFFER_FMT_TYPE_FLOAT) {
((ai_float *)in_data)[i] = val;
} else { /* AI_BUFFER_FMT_TYPE_Q */
/* Scale the values in the range [-2^M, 2^M] */
val *= max_;
/* Convert float to Qmn format */
const ai_i32 tmp_ = AI_ROUND(val * scale_, ai_i32);
in_data[i] = AI_CLAMP(tmp_, -128, 127, ai_i8);
}
}
I can't understand why the input buffer is filled with random data instead of the original input data?
I expect that all this code need to be commented, am I right?
Labels:
- Labels:
-
STM32CubeMX
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0