2025-02-24 3:27 AM
Hi,
I am using STM32N6570-DK kit. I have an example project for image classification, but it is designed for STM32CubeIDE. I want to port this project to Keil ( in order to use the ARM Compiler). Could you please provide the project file so it can be executed on Keil?
2025-03-12 9:15 AM
Hello @VasuV ,
Sorry for the late answer,
Sadly we don't have an example with Keil, but you aren't the first to ask so I escalated the demand to the dev teams.
They might work on one, but I cannot promise...
Have a good day,
Julian
2025-03-12 11:37 PM
Thanks for your reply, Julian.
Example code also doesn't have a .ioc file. If we want to use the example code as Base code to develop other use cases it gets hard to configure the project HAL layers manually in barematel.
It would be great if you could provide the .ioc file for the same example as well so we can get started with development.