2025-08-16 1:48 AM - last edited on 2025-08-18 6:59 AM by Julian E.
Hi @Julian E.
While following along the tutorial:
How to build an AI application from scratch on the... - STMicroelectronics Community
after selecting the x-cube-ai package a described, I see that the default is enabled for fsbl and I cannot change that to application in the UI. Tried deselecting fsbl first, but it doesn't work.
Then I downloaded your ioc and there it is set to applciation - but this cannot be changed to anything else (for example to fsbl) - basically the checkboxes cannot be changed.
Have you seen this?
What am I doing wrong?
Also, I get this warning:
I have installed all the firmwares by first downloading as zip and then installing from local in CubeMX
I have downloaded v1.1.1, v1.1.0 and v1.2.0 as well as the patch file from ST website and still get the same warning
Update 17/08/25:
With the downloaded ioc file, I see some clock config errors as:
Is this okay?
Also - please explain what should be the input to validation dataset for the AI suite UI.
I went ahead and generated code anyway, even though there were some warning about wrong configurations
I also keep getting these from the AI window
- NPU not-selectable in the RIF tab (using the DK_tuto.ioc)
Best Regards
2025-09-05 12:28 AM
Hello @ERROR,
Yes, for some reason, this parameter tends to change on its own. I have no idea why, I will report it in an internal ticket.
Have a good day,
Julian
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.