cancel
Showing results for 
Search instead for 
Did you mean: 

Is the ISM330ISN the only product with the ISPU? If yes, all those can be programmed with the NEAI studio?

Evelina CAMILLERI
ST Employee
 
1 REPLY 1
Luca SEGHIZZI
Senior

There are more products using the ISPU on top of the one used for the webinar, however, the ISM330ISN is the only one which can be programmed using the NEAI studio SW tool. The other products are the ISM330IS which is the industrial version of an ISPU device that doesn't have the possibility to program with the NEAI, but only with C language and we have the same for the LSM6DSO16IS which is the consumer part number, these two part numbers can be used easily with the X-CUBE-ISPU software package.