cancel
Showing results for 
Search instead for 
Did you mean: 

Is ST better or worse than other MEMS based sensors for Artificial Intelligence offer?

Evelina CAMILLERI
ST Employee

 [webinar - Program decision trees in sensors with a Machine Learning Core]

1 REPLY 1
Evelina CAMILLERI
ST Employee

The traditional MEMS components on the market are, as of today, without any capabilities to process Machine Learning algorithms with a negligible power consumption. 

ST 6-axis Inertial Modules such as LSM6DSOX, LSM6DSRX and ISM330DHCX are the first ones with a dedicated logic for Machine Learning algorithms with undisputed low power efficiency. 

Apple-to-apple comparison of ST sensors with MLC and other MEMS based sensors is not straight-forward in this moment. For above reason, we think, these new generation of 6-axis inertial modules are the best-in-class solution with undisputed flexibility for the system power consumption. Finally, I want to remember that a complete toolbox chain offer the possibility to implement AI algorithms in an easy and simple way without writing any single line of code.