cancel
Showing results for 
Search instead for 
Did you mean: 

Integration of AI in old CubeMX project

ElisaWeber
Associate

Hello everybody,

I started to use the AI Cube MX extension and developed an application on the NUCLEO-F746ZG Board. It all worked very well.

Now I am trying to integrate this small application into a bigger, existing project.

There seems to be a problem with the Init function of the AI, it causes a reset after a few seconds.

There are a  few possible problems I identified:

- the project was configured with a CubeMX Version the AI extension is not compatible with

- the clock configurations of the two project parts seem to clash (HSE_ON vs. HSE_BYPASS)

Does anyone have experience with that?

Does anyone know any clock configuration etc. that the AI extension is compatible with? I cannot find much in the documentation...

 

 

0 REPLIES 0