2025-02-17 3:27 AM
I am using the STEVAL-C34KAT2 with the STEVAL-STWINBX1 which is running the software FP-SNSDATALOG2 V3.0.0.
Do I need to change anything in the FP-SNSDATALOG2 V3.0.0 software ?
Or does the software automatically detect the STEVAL-C34KAT2 board ?
Does anything need to be added to the device_config.json file ?
I have read the user manual for the STEVAL-C34KAT2, it explains how to connect the board but there's no explanation on how to use it in terms of software.
Is it just plug and play or are there extra steps required ?
Solved! Go to Solution.
2025-02-17 7:25 AM
Hello @johngj
STEVAL-C34KAT2 is automatically detected and supported by DATALOG2 firmware for STEVAL-STWINBX1.
Simply plug the expansion board to the STWVAL-STWINBX1, power up the board (by plugging USB or using battery) and start the logging (via SD card or USB using the Python-based SDK).
Best regards,
Simone
2025-02-17 7:25 AM
Hello @johngj
STEVAL-C34KAT2 is automatically detected and supported by DATALOG2 firmware for STEVAL-STWINBX1.
Simply plug the expansion board to the STWVAL-STWINBX1, power up the board (by plugging USB or using battery) and start the logging (via SD card or USB using the Python-based SDK).
Best regards,
Simone