cancel
Showing results for 
Search instead for 
Did you mean: 

Generate file .ucf with NanoEdgeAI

ChristianValota
Associate II

Good afternoon,

I want to upload a Machine Learning algorithm on the ISPU part of the LSM6DSO16IS. My alghoritm has to identify is the subject is stationary, walking or running. I used NanoEdgeAI Studio to develop the classification algorithm. By doing this I obtain these files, but don't the .ucf file, which is the file that I have to upload on the ISPU part of the sensor. By uploading this files on the Nucleo, it performs the classification correctly, but I want the classification to be done by the sensor. Which is the easyest way to obtain it starting from the files that I obtained? 

 

Screenshot 2024-12-10 161113.png

1 ACCEPTED SOLUTION

Accepted Solutions
Julian E.
ST Employee

Hello @ChristianValota,

 

It seems you didn't select the ISPU as target in your project settings.

The ISPU is only available for anomaly detection in NanoEdge under the name ISM330ISN.

So, I don't think you can do your multiple classes classification...

JulianE_0-1733846841253.png

You can look at this tutorial if you decide to do anomaly detection with the ISPU to understand how to deploy a model: https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Anomaly_Detection_library_for_ISPU 

 

You may take a look to the Tool MEMS Studio instead: MEMS-Studio - Software solution for MEMS sensors with graphical no-code design of algorithms and development of embedded AI features - STMicroelectronics

(I never used it, so I am not sure)

 

Have a good day,

Julian

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Julian E.
ST Employee

Hello @ChristianValota,

 

It seems you didn't select the ISPU as target in your project settings.

The ISPU is only available for anomaly detection in NanoEdge under the name ISM330ISN.

So, I don't think you can do your multiple classes classification...

JulianE_0-1733846841253.png

You can look at this tutorial if you decide to do anomaly detection with the ISPU to understand how to deploy a model: https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Anomaly_Detection_library_for_ISPU 

 

You may take a look to the Tool MEMS Studio instead: MEMS-Studio - Software solution for MEMS sensors with graphical no-code design of algorithms and development of embedded AI features - STMicroelectronics

(I never used it, so I am not sure)

 

Have a good day,

Julian

 

 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.