cancel
Showing results for 
Search instead for 
Did you mean: 

Assistance with TensorFlow-Lite Model Porting on NUCLEO-F401RE Board

Sanchali
Associate

Hi,

I'm encountering an issue while porting a trained TensorFlow-Lite model, obtained from a research paper, onto a NUCLEO-F401RE board. The process goes smoothly when analyzing and validating the code on my desktop, generating the code, and downloading it to the board. However, when I attempt to perform a "validate of target," I receive an "Invalid firmware" error (screenshot attached). The model is neural network based on U-Net architecture with shallow structure, single-channel input, and output.

Board used: NUCLEO-F401RE

STM32MX : Version 6.12.0

STM32CubeIDE : Version: 1.16.0

Could you please provide guidance on how to resolve this issue? Any suggestions for modifications or troubleshooting steps would be greatly appreciated.

Thank you!

1 REPLY 1
fauvarque.daniel
ST Employee

Please verify in the log that the firmware has been correctly compiled and flashed on the target

You can retreive the logs in ~/.stm32cubemx/STM32CubeMX.log

Regards

Daniel


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.