cancel
Showing results for 
Search instead for 
Did you mean: 

Additional Softwares is not displayed in CubeMX 5.0.1

NKryl
Associate

Hello!

My problem is that I don't see the components in the Additional Software menu.

I did everything strictly according to the instructions specified in the official video "Getting Started with STM32Cube.AI". Components installed as shown.

CubeMX reinstalled, the computer rebooted, but it did not help. Touching Refresh button also has no any effect.

What could be the problem?

3 REPLIES 3
fauvarque.daniel
ST Employee

X-Cube-AI is supported only on Cortex M4 and M7 devices.

If you choose an MCU that has a Cortex M0 or M0+ X-Cube-AI won't be shown in the additional software components.

Please start your project with an STM32F3, STM32F4, STM32F7 or STM32H7 device.

If you activate the AI extended filter in the mcufinder you'll have the supported MCUs

Regards

Daniel


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

I tried with STM32F4 and STM32F7 MCU's, that 100% supports AI functionality.

OBorz.1
Associate II

Hello, i´ve the same problem. I use a STM32H747I-DISCO. How can i fix this problem?