2024-03-08 12:26 AM
I want to flash and debug using SPC5-UDESTK 5.02.04 on to the board SPC5746CBMKU6. This controller configuration is not given in the tool. So I have created new configuration for this board. Now I have tried to connect to target board. But it is failing to establish connection.
Connection and power supply is good(Tool LED glows). May be problem with target configuration.
Attaching failed report and new target configuration file(in .txt, as .cfg is not supported here). Kindly provide the target configuration file for SPC5746CBMKU6, if you have. Or suggest edits in current file.
Solved! Go to Solution.
2024-03-08 05:52 AM
Hello ,
The board SPC5746CBMKU6 is a processor coming from NXP side.
I recommend to check with them.
I do not known if there is PLS Ftdi in this board.
Best regards
Erwan
2024-03-08 05:52 AM
Hello ,
The board SPC5746CBMKU6 is a processor coming from NXP side.
I recommend to check with them.
I do not known if there is PLS Ftdi in this board.
Best regards
Erwan