2014-10-01 04:03 AM
Hello,
Can anybody explain me the exact difference between the ADC precision channels and the ADC standard channels for a SPC560B? I read the ADC section within the reference manual, but I did not find any differences. Best regards, PatrikSolved! Go to Solution.
2014-10-01 06:12 AM
Hello Patrik,
the precision channels are internally multiplexed and have a better accuracy.Comparing the standards one, the precision channels are mapped on input only I/O cells.(cf Functional Port Pin description)The implicit channel conversion priority in the case in which all channels are selected is thefollowing: Precision[0:x], Standard[0:y], External[0:z]. Best regards Erwan2014-10-01 06:12 AM
Hello Patrik,
the precision channels are internally multiplexed and have a better accuracy.Comparing the standards one, the precision channels are mapped on input only I/O cells.(cf Functional Port Pin description)The implicit channel conversion priority in the case in which all channels are selected is thefollowing: Precision[0:x], Standard[0:y], External[0:z]. Best regards Erwan