cancel
Showing results for 
Search instead for 
Did you mean: 

Processor is in unknown state!

Wilhelm Bairlein
Associate
Posted on January 08, 2018 at 16:10

hello everybody,

we use the SPC56EL70 discovery board with Spc5 studio as IDE and UDE STK - 4.8 as Debugger.

Today we got the following failure message - please see the following picture.

0690X00000609O6QAI.png

The only thing we changed was the additional usage of the A/D-port E12. After downloading the extended code we got the above failure message. Now we can�t flash the SPC with another source code.

Please let us know how we can put the SPC back into operation.

Thanks in advance.

#processor-in-unknown-state
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
david tomsa
Associate III
Posted on January 09, 2018 at 06:59

Hi,

you can try the following: Interface Setup -> Connect and choose under connect: Keep application running. 

View solution in original post

3 REPLIES 3
david tomsa
Associate III
Posted on January 09, 2018 at 06:59

Hi,

you can try the following: Interface Setup -> Connect and choose under connect: Keep application running. 

Posted on January 09, 2018 at 10:10

Hi ,

Yes , in LSM (Lock Step Mode) , you should update your debug configuration

Posted on January 09, 2018 at 15:15

Hi Erwan,

how can I update the debug configuration respectively which settings do you mean?