cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with SPI configuration - data is not getting transmitted

sjpatel19922
Associate III
Posted on April 07, 2017 at 20:38

Hello, I would like to know what is wrong with my current configuration of SPI module. I can see data in the TX FIFO, but its not getting transmitted.

I am using the

SPC570S40E1 microcontroller.

SPI Port Configuration

void Initialize_SPI_Port(void)
{
// Using DSPI 0
 // DSPI0_CS -- PA[0] , Pin #2, PAD[0]
 SIUL2.MSCR_IO[0].B.SSS = PAL_SPC5_SSS(1);

 // DSPI0_SCK -- PA[3] , Pin #3, PAD[3]
 SIUL2.MSCR_IO[3].B.SSS = PAL_SPC5_SSS(1);

 // DSPI0_MISO -- PA[4], Pin #4, PAD[4]
 SIUL2.MSCR_IO[4].B.IBE = 1;
 SIUL2.MSCR_MUX[624-512].R = PAL_SPC5_SSS(1);
 // DSPI0_MOSI -- PA[7], Pin #5, PAD[7]
 SIUL2.MSCR_IO[7].B.SSS = PAL_SPC5_SSS(1);
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

SPI Module conffiguration

void Initialize_DSPI0(void)
{
 // Configure DSPI0 Module Configuration Register ( DSPI0_MCR )
 // MSTR - 0 , Master mode
 // CONT_SCKE - 0 , Continuous SCK disabled
 // DCONF - 00 , SPI
 // FRZ - 0 , Do not halt serial transfers in debug mode
 // MTFE - 0 , Modified Timing Format disabled
 // ROOE - 0 , (Receive FIFO Overflow Overwrite) Incoming data is ignored
 // PCSIS0 - 1 , Inactive state of PCS0 is high
 // MDIS - 1 , Allow external logic to disable DSPI clocks
 // DIS_TXF - 0 , TX FIFO enabled
 // DIS_RXF - 0 , RX FIFO enabled
 // XSPI - 0 , Normal SPI Mode
 // FCPCS - 1 , Fast Continuous PCS mode.
 // PES - 0 , SPI frame transmission continues
 // HALT - 0 , Start transfers
 DSPI_0.MCR.R = 0x10004;
 // Configure CTAR0 and CTAR1 ( Clock and Transfer Attributes ) Register
 // Two transfer attributes used. CTAR0 configured for 16-bit frame size. CTAR1 configured for 8-bit frame size.
 // DBR - 0 , Baud rate not doubled
 // FMSZ(for CTAR0) - 1111 , Frame size set to FMSZ + 1 or 16 bits
 // CPOL - 0 , Clock Polarity - Inactive state value of SCK is low
 // CPHA - 0 , Data is captured on the leading edge of SCK and changed on the following edge
 // LSBFE - 0 , MSB is transferred first
 // PCSSCK - 00 , PCS to SCK Prescaler value is 1
 // PASC - 00 , Sets the delay between last SCK edge to negation of CS, 00 sets the Prescaler value to 1
 // PDT - 00 , Sets the delay between negation of PCS at end of frame to assertion beginning of next frame, 00 - Prescaler set to 1
 // PBR - 00 , Baud Rate Prescaler, set to 2. Available values - 2,3,5, and 7
 // CSSCK - 0000 , PCS to SCK Delay Scaler set to 2
 // ASC - 0000 , Scaler value for the After SCK Delay, set to 2
 // DT - 0000 , Scaler value set to 2
 // BR - 0011 , Baud Rate scaler set to 8
 /* ------------ Calculation ------------------------

 SPI Baud Rate = (Fp / PBR) * ( [1 + DBR]/BR ) , Fp = Peripheral Clock / AC0_DC3 = 64/1 = 64Mhz
 = (64/2) * ( [1]/8 )
 = 64/16
 = 4Mhz
 
 */
 DSPI_0.CTAR[0].R = 0x78000003;
 DSPI_0.CTAR[1].R = 0x38000003;

}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

0690X00000606iNQAQ.png #spc570s #spi
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 ACCEPTED SOLUTION

Accepted Solutions
sjpatel19922
Associate III
Posted on April 07, 2017 at 22:59

Figured out what the problem was. I didn't realize I had it configured as a slave device.

View solution in original post

1 REPLY 1
sjpatel19922
Associate III
Posted on April 07, 2017 at 22:59

Figured out what the problem was. I didn't realize I had it configured as a slave device.