2025-04-02 12:20 AM - last edited on 2025-04-02 8:05 AM by FSPIL
Hi
We are using STEVAL -TTM001V1 Kit which consists of L9907 driver and trying to interface it with STEVAL-TTM002V1 Controller board (SPC560P50L3) to run the O-Drive 5312 Motor.
We are using the sample program SPC560P50L3_MotorControl_STEVAL-TTM001V1 from application library to run the motor.
We have changed the motor parameters according to O-Drive 5312 motor in the motor settings of the motor control component.
Then generated the application code in Observer + PLL ( Sensorless ) mode to run the motor. We are not getting any waveform in the PWM pin when checked with an oscilloscope.
Are we missing out anything else ?
2025-04-03 10:32 AM
Hi,
We do not support STEVAL-TTM001V1 kit and STEVAL -TTM002V1 in AutoDevKit.
The suggested kit with software are:
AEK-MOT-3P99081 or AEK-MOT-3P9908M
The User Manual included in st.com will give some basic indication on how to set the motor control library:
Best Regards,
AutoDevKit Team