hello,in order to fabricate a SPC570S40E1 microcontroller board could be worth reading two Application Notes AN4721 "Hw recommendations for SPC570Sx device family"AN5010 "SPC570Sx Getting Started"Both of them can be downloaded from SPC57 0S line MCUs...
Hello,unfortunately using the SR5E1 is not possible to understand the core running directly reading an unique Id; as you suggested is it possible to do a software workaround for example reading the address of the Vector Table that will be different b...
Hello,unfortunately using the SR5E1 is not possible to understand the core running directly reading an unique Id; as a workaround it is possible to do this via software for example reading the address of the Vector Table that will be different betwee...