2022-05-24 4:09 AM
Hello I'm sharan from yali mobilities. Here we are shifting from old spc5 studio to latest version spc5 studio 6.0. For testing I2C, I have used Arduino as a slave device. The programme which I have writen is attached as image. Arduino sends a inter value when an request event is occured. The programme runs in old spc5 studio, but it's not working in spc5 studio 6.0. I have used same configurations, setups and same board.
I have tried I2C write function it works properly for all the devices, which I have tested. If any one knows the solution kindly reply.
Thank you for reading.
Solved! Go to Solution.
2022-06-12 11:18 PM
Hello,
R&D found a regression on I2C HW, we will come back to you as soon as the fix is ready.
Best regards,
-Olivier
2022-07-12 11:50 PM
Is there any update regarding the I2C driver?
2022-08-02 2:03 AM
Hello,
I asked to R&D but I had no news yet.
I may not have an answer until the end of august.
Best Regards
2022-09-16 6:24 AM
Hello,
Now, is it fixed or not. Kindly reply.
Thank you
2022-09-19 2:06 AM