cancel
Showing results for 
Search instead for 
Did you mean: 

i cant find GTM344 details in SPC58NN manual,any one knows where can find that?

szhan.7
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
ODOUV.1
ST Employee

the specification can be found on Bosch GTM web site https://www.bosch-semiconductors.com/ip-modules/gtm-platform/gtm-generic-timer-ip-module/ "GTM IP - Specification V3.1.5.1".

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

You will find the description in RM0421, section 45.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ODOUV.1
ST Employee

you may find more details in application notes AN5552 AN5693 or AN5695 downloadable on www.st.com

Best regards

ODOUV.1
ST Employee

the specification can be found on Bosch GTM web site https://www.bosch-semiconductors.com/ip-modules/gtm-platform/gtm-generic-timer-ip-module/ "GTM IP - Specification V3.1.5.1".

thanks�?

WAnth.1
Associate

This manual is designed to provide the user with an understanding of the RSK hardware functionality, and electrical characteristics. It is intended for users designing sample code on the RSK platform, using the many different incorporated peripheral devices. The manual comprises of an overview of the capabilities of the RSK product, but does not intend to be a guide to embedded programming or hardware design. Further details regarding setting up the RSK and development environment can found in the tutorial manual. 

https://knifeplatoon.com0693W00000Une8NQAR.png