cancel
Showing results for 
Search instead for 
Did you mean: 

How to use eMIOS library for input capture

Yali Mobilities
Associate III

Hi,

   I'm using SPC58EC Disp board. I want to use ultrasonic sensors with it. For that I have to config eMIOS as input capture mode. So, is there any example to config the libraries. If any kindly give it with some instructions. Thank You

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Hello ,

you can find in attachment the application SPC56D with HCSR04 Ultrasonic sensor.

You should adapt it based of the datasheet of your sensor and the RM SPC58EC Disp Board.

to use EMIOS as input capture mode is a good idea to have a good accurate measure.

You can import it in SPC5Studio.

Best regards

Erwan

View solution in original post

5 REPLIES 5
Erwan YVIN
ST Employee

Hello ,

Which ultrasonic sensor do you use ?

i recommend to configure the EMIOS

There is an old example on emios configuration on HCSR04 (Mass Masket device) with emios configuration on SPC5Studio side.

I can retrieve for you if you want ;-)

Best regards

Erwan

Thanks for your reply kindly send that example, it will be usefull for us.

Erwan YVIN
ST Employee

Hello, Which Ultrasonic sensor do you use ?

Best Regards

Erwan

I'm using JSN-SR04T ultrasonic sensor. Thank you.

Erwan YVIN
ST Employee

Hello ,

you can find in attachment the application SPC56D with HCSR04 Ultrasonic sensor.

You should adapt it based of the datasheet of your sensor and the RM SPC58EC Disp Board.

to use EMIOS as input capture mode is a good idea to have a good accurate measure.

You can import it in SPC5Studio.

Best regards

Erwan