2022-06-22 12:15 AM
Hi,
I'm using SPC58EC Disp board. I want to use ultrasonic sensors with it. For that I have to config eMIOS as input capture mode. So, is there any example to config the libraries. If any kindly give it with some instructions. Thank You
Solved! Go to Solution.
2022-06-28 7:31 AM
Hello ,
you can find in attachment the application SPC56D with HCSR04 Ultrasonic sensor.
You should adapt it based of the datasheet of your sensor and the RM SPC58EC Disp Board.
to use EMIOS as input capture mode is a good idea to have a good accurate measure.
You can import it in SPC5Studio.
Best regards
Erwan
2022-06-23 8:35 AM
Hello ,
Which ultrasonic sensor do you use ?
i recommend to configure the EMIOS
There is an old example on emios configuration on HCSR04 (Mass Masket device) with emios configuration on SPC5Studio side.
I can retrieve for you if you want ;)
Best regards
Erwan
2022-06-25 12:05 AM
Thanks for your reply kindly send that example, it will be usefull for us.
2022-06-27 8:05 AM
Hello, Which Ultrasonic sensor do you use ?
Best Regards
Erwan
2022-06-27 10:25 PM
I'm using JSN-SR04T ultrasonic sensor. Thank you.
2022-06-28 7:31 AM
Hello ,
you can find in attachment the application SPC56D with HCSR04 Ultrasonic sensor.
You should adapt it based of the datasheet of your sensor and the RM SPC58EC Disp Board.
to use EMIOS as input capture mode is a good idea to have a good accurate measure.
You can import it in SPC5Studio.
Best regards
Erwan