2018-12-03 05:35 AM
I have data which i need to store in eeprom,but i am facing following issue:
Solved! Go to Solution.
2018-12-11 08:01 AM
Hello Aditya ,
Did you use EEPROM components from SPC5Studio ?
if yes , there is a useful document in the document (cf screenshot)
Best regards
Erwan
2018-12-11 08:01 AM
2019-01-07 10:38 PM
Thanks @Erwan YVIN , I am able to read,write and erase EEPROM.
But , I am able to do it only when it is debug mode.
And in Normal rum mode, i am able to read only , but not able to erase and write.
Please help me with this.
2019-01-10 12:57 AM
Hello Aditya ,
Could you confirm the family used ?
There are some examples in Read, Erase and Write in
SPC560BCxx EE Test Application\
SPC560BCxx_RLA EE Test Application\
SPC560Bxx EE Test Application for Discovery\
SPC560Bxx_RLA EE Test Application for Discovery\
SPC560Dxx EE Test Application for Discovery\
SPC560Dxx_RLA EE Test Application for Discovery\
SPC560Pxx EE Test Application for Discovery\
SPC560Pxx_RLA EE Test Application for Discovery\
SPC563Mxx EE Test Application for Discovery\
SPC563Mxx_RLA EE Test Application for Discovery\
SPC564Axx EE Test Application for Discovery\
SPC564Axx_RLA EE Test Application for Discovery\
SPC56ECxx EE Test Application\
SPC56ECxx_RLA EE Test Application\
SPC56ELxx EE Test Application for DiscoveryPlus\
SPC56ELxx_RLA EE Test Application for DiscoveryPlus\
SPC570Sxx_RLA EE Test Application for Discovery\
SPC574Sxx_RLA EE Test Application\
SPC582Bxx_RLA EE Test Application for Discovery\
SPC584Bxx_RLA EE Test Application for Discovery\
SPC58ECxx_RLA EE Test Application for Discovery\
SPC58xExx_RLA EE Test Application\
SPC58xGxx_RLA EE Test Application for Discovery\
SPC58xNxx_RLA EE Test Application\
Best regards
Erwan