2021-03-11 2:44 AM
Hello! I've tried to modify UTEST DCF Client but some questions (below) appeared to me.
Sorry, I'm new here and maybe I've done something wrong. This is mine post below:
https://community.st.com/s/question/0D53W00000NBVl1SAH/enabling-lockstep-core-in-spc570s-mcu
Upd:
I've found AN4557. And now I really don't undestand anything in the DCF records. How to make CS field? etc...=(
Thank you,
Nikolay Mannhof
Solved! Go to Solution.
2021-06-03 2:09 AM
Hello Manhof ,
There is an interesting document in NXP side
it is the same IP
to modify a record , it is OTP.
there is a possibility to overwrite it cf chap 3.5
Best regards
Erwan
2021-04-06 1:44 AM
Hello,
I remind about this question.
Thank you,
Nikolay Mannhof
2021-04-13 10:29 PM
Hi Nikolay
I was able to read and write this area using the Multilink Universal + ICDPPCNEXUS eval version bundle.
As in your case, the UTEST DCF records area is empty. Tell me, is your processor starting up? I do not get to main (), init process loops on some checks.
Best regards,
Zharov Maxim
2021-04-14 12:55 AM
Hi Maxim.
Yes, MCU starting up. But only if it clocking from IRC. Try to disable in all RUN modes XOSC start.
Clocking from XOSC isn't starting due to internal loading capacitors. Capacitors's value changeable via DCF UTEST Flash memory area.
Thank you,
Nikolay Mannhof
2021-04-19 11:48 PM
Hi Nikolay
My result - processor starts with quartz 8 & 16 Mhz without any change of UTEST DCF. Significant factors was 1) tracing of 1.2 V line (general polygon, 0.1 uF+2.2 uF at each pin), and 2) proper peripherial init in programm.
Best regards,
Zharov Maxim
2021-06-03 2:09 AM
Hello Manhof ,
There is an interesting document in NXP side
it is the same IP
to modify a record , it is OTP.
there is a possibility to overwrite it cf chap 3.5
Best regards
Erwan