2020-11-05 1:19 AM
Hi,
I am prototyping on a SPC570S-DISP development board, and I am trying to enable the checker core in the MCU. I read the technical reference manual, and it has stated that the checker core can be enabled from the UTEST DCF memory registers. How can I access these registers from the SPC5 application, because such a setting is not available in the configuration GUI. Furthermore, I would really appreciate if I could get some advice as to how to access other registers as well.
Thank you.
Nisal
Solved! Go to Solution.
2021-06-03 7:03 AM
Hello ,
you can not access by GUI Settings
you need to access by adding some constants
/*UTEST DCF pattern */
#define UTEST_DCF_records 0x00400308 /* just after DCF_start_Record */
#define UTEST_DCF_PASS_ADDR 0x00400308 /* DCF START */you can try to access after locking UTEST Address Space
/**************************************************************************/
/* Lock to Protect UTest Address Space */
/**************************************************************************/
test_string_print(&SD1, "Lock UTEST Address Space: ");
returnCode = GetLock(&ssdConfig, C55_BLOCK_UTEST, &blkLockState);
if (C55_OK != returnCode)
{
ErrorTrap(returnCode);
}
if (!(blkLockState & 0x00000001))
{
returnCode = SetLock(&ssdConfig, C55_BLOCK_UTEST, LOCK_ALL_BLOCKS);
if (C55_OK != returnCode)
{
ErrorTrap(returnCode);
}
}
test_string_print(&SD1, "OK!\n\r");Example in Flash Test Application
Best Regards
Erwan
2021-03-11 2:28 AM
Hi all! I'm also trying to change UTEST DCF in SPC570S40 (but I want to change XOSC LF_EN bit value).
In RM0349 on the page 260 I see it's Reset value. How can I read it? UTEST Flash memory with the same address is empty.
If I'm flashing address 0x00400308 but nothing changes. How can I check current values which stored in this memory?
Thank you,
Nikolay Mannhof.
2021-06-03 7:03 AM
Hello ,
you can not access by GUI Settings
you need to access by adding some constants
/*UTEST DCF pattern */
#define UTEST_DCF_records 0x00400308 /* just after DCF_start_Record */
#define UTEST_DCF_PASS_ADDR 0x00400308 /* DCF START */you can try to access after locking UTEST Address Space
/**************************************************************************/
/* Lock to Protect UTest Address Space */
/**************************************************************************/
test_string_print(&SD1, "Lock UTEST Address Space: ");
returnCode = GetLock(&ssdConfig, C55_BLOCK_UTEST, &blkLockState);
if (C55_OK != returnCode)
{
ErrorTrap(returnCode);
}
if (!(blkLockState & 0x00000001))
{
returnCode = SetLock(&ssdConfig, C55_BLOCK_UTEST, LOCK_ALL_BLOCKS);
if (C55_OK != returnCode)
{
ErrorTrap(returnCode);
}
}
test_string_print(&SD1, "OK!\n\r");Example in Flash Test Application
Best Regards
Erwan