2021-02-11 03:02 AM
I am using SPC58EC MCU board to send some through Ethernet , For this one I tried to generate new project inside that I selected the network section , Inside I choose ping project.
Can any body suggest how to configure Ethernet driver?
Solved! Go to Solution.
2021-02-19 05:52 AM
hello ,
There is a nice example in SPC5Studio 6.0
SPC58ECxx_RLA Network Ping Test Application for Discovery
Best regards
Erwan
2021-02-19 05:52 AM
hello ,
There is a nice example in SPC5Studio 6.0
SPC58ECxx_RLA Network Ping Test Application for Discovery
Best regards
Erwan
2021-02-22 10:23 PM
Thank You Erwan.
I tried this it work successfully , But I want to receive some data on SPC58EC board from host system (Linux).
Please suggest me how can I achieve this task.
Regards
Ganesh.
2021-09-09 03:35 AM
Hi Kmaza,
Were you able to establish communication via Ethernet between two SPC58 boards or between board and Host PC?
I would like to realize something similar, but I still haven't been able to find any answers by studying the Network Ping Test application. Dear @Erwan YVIN There is an example in which I can send segment(TCP) or Datagram(UDP) from SPC58EC-DISP?
Thank you both,
Vincenzo