2024-10-08 3:25 AM
Hello team,
I am currently working on configuring the GPT (General Purpose Timer) MCAL module for the SPC58NN84 microcontroller. While I have successfully configured PIT channels 0 and 1 for my project, I am encountering an error related to RTC (Real-Time Clock) channels during compilation.
Error Message:
In file included from C:/STMicroelectronics/SPC58XE-Nxx_MCAL40_101_Signed/Gpt_TS_T2D42M10I1R0/src/Gpt_NonASR.c:79:0:
C:/STMicroelectronics/SPC58XE-Nxx_MCAL40_101_Signed/Gpt_TS_T2D42M10I1R0/include/Gpt_LLD.h:386:52: error: 'GPT_RTC_CHAN_NUM' undeclared here (not in a function)
extern VAR(uint8, GPT_VAR) GPT_LLD_RTC_HardwareMap[GPT_RTC_CHAN_NUM];
Findings:
/* FOR GTM PIT STM RTC */
/**
* @brief The number of STM HW channels
*/
#define GPT_STM_CHAN_NUM 12U
/**
* @brief The number of PIT HW channels
*/
#define GPT_PIT_CHAN_NUM 9
/**
* @brief The number of GTM HW channels
*/
#define GPT_GTM_CHAN_NUM 48
Given these findings, I would like to ask the community for guidance on how to resolve the compilation error related to GPT_RTC_CHAN_NUM.
Specifically:
What steps should I take to ensure that my project compiles without errors related to RTC?
Are there any known issues or specific configurations I should be aware of when working with the SPC58NN84?
Any insights or suggestions would be greatly appreciated!
Thank you in advance for your help!
Veer