2022-05-16 6:20 AM
In the schematic of the ethernet configuration it is indicated that 3 components are not assembled: R28, R33 and R120. My question is, should I solder them for it to work?
Solved! Go to Solution.
2022-05-16 6:48 AM
Hello,
from README.TXT
It needs to configure the network component providing the networking configuration:
i.e: MAC Address, IP static Address.
Open a console and ping from a remote host to the IP address configured for the board.
Fit the following jumpers to configure the network:
JP5:
ETH_PWR -> [3 - 4]
RESET -> [5 - 6]
ETH_TX_CLK -> [7 - 8]
ETH_TXD_0 -> [9 - 10]
ETH_TXD_1 -> [11 - 12]
ETH_TXD_2 -> [13 - 14]
ETH_TXD_3 -> [15 - 16]
ETH_TX_EN -> [17 - 18]
ETH_MDIO -> [19 - 20]
ETH_MDC -> [21 - 22]
ETH_COL -> [23 - 24]
ETH_CRS -> [25 - 26]
ETH_RX_ER -> [27 - 28]
ETH_RX_DV -> [29 - 30]
ETH_RXD_0 -> [31 - 32]
ETH_RXD_1 -> [33 - 34]
ETH_RXD_2 -> [35 - 36]
ETH_RXD_3 -> [37 - 38]
ETH_RX_CLK -> [39 - 40]
JP50: FIT
Do not forget to plug a cable.
Regards.
2022-05-16 6:25 AM
Hello,
no need to solder any resistor.
Please close the jumper in connector JP5 from 5 to 39.
Regards.
2022-05-16 6:32 AM
I'd expect not. Would depend on what pins you end up using on the interface. Watch PWR_DOWN/INT and COL/PHYAD0
The JP5 needs to have pins being used for the MII/RMII bridged (jumpered).
Check any related README.TXT notes or comments in the example code.
2022-05-16 6:37 AM
Still doesn't work, even the leds of the RJ45 connector don't turn on
2022-05-16 6:48 AM
Hello,
from README.TXT
It needs to configure the network component providing the networking configuration:
i.e: MAC Address, IP static Address.
Open a console and ping from a remote host to the IP address configured for the board.
Fit the following jumpers to configure the network:
JP5:
ETH_PWR -> [3 - 4]
RESET -> [5 - 6]
ETH_TX_CLK -> [7 - 8]
ETH_TXD_0 -> [9 - 10]
ETH_TXD_1 -> [11 - 12]
ETH_TXD_2 -> [13 - 14]
ETH_TXD_3 -> [15 - 16]
ETH_TX_EN -> [17 - 18]
ETH_MDIO -> [19 - 20]
ETH_MDC -> [21 - 22]
ETH_COL -> [23 - 24]
ETH_CRS -> [25 - 26]
ETH_RX_ER -> [27 - 28]
ETH_RX_DV -> [29 - 30]
ETH_RXD_0 -> [31 - 32]
ETH_RXD_1 -> [33 - 34]
ETH_RXD_2 -> [35 - 36]
ETH_RXD_3 -> [37 - 38]
ETH_RX_CLK -> [39 - 40]
JP50: FIT
Do not forget to plug a cable.
Regards.
2022-05-16 6:49 AM
Is JP50 powering the Ethernet side hardware?
Probe a couple of points checking you get voltage and can see clocks.
2022-05-16 7:11 AM
Yes, the JP50 is correct. And i have the clock pulses. Now, after reprogramming the leds are blinking, but I can´t ping