cancel
Showing results for 
Search instead for 
Did you mean: 

Debug Port Fail in SPC5xx

swarnkarankit47
Associate II
Posted on June 08, 2018 at 07:14

I am working on SPC563M64 controller. I have started working on shadow flash now. But during testing of shadow flash code I got debug port fail error while trying to connect to controller. I think the board is permanently reset and I am not able to connect to my board again. What can I do ? I have also tried the sequence of commands in a sequence listed below but still I was not able to connect to controller :

1. system.option.cpu   

2.SYStem.Option.KEYCODE 0xFEEDFACECAFEBEEF

3. system.up.

Please tell me what is this issue is ?

#spc5x
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Erwan YVIN
ST Employee
Posted on June 08, 2018 at 09:59

Hello Ankit ,

You are using TRACE32 lautechbach ..

Have you updated the shadow flash ?

could you try to click on Reset Button of your board in trying to connect the debugger in the same time .

Maybe , there is a sort of reset escalation.

     Best Regards

                      Erwan

Posted on June 08, 2018 at 10:31

Yes I updated shadow flash and after that I did reset and from then this problem is coming.

I tried to connect to board while press the reset button at the same time but error showed that ' target reset failed '.