cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a new SPC5 application from Scratch

NDinu.1
Associate II

Hi,

I am using a SPC570S-DISP development board, and I am trying to create a new application form that. I have tested out a few example application given in the IDE, and they work fine.

Now I want to develop such an application from scratch. However, there seem to be no guide as such, showing the necessary step to follow in order to properly configure the application. I have also referred the Help section.

One problem that I came across is that, in the MCU wizard, I am unable to configure any of the peripherals. When I click on one of the peripherals, no options seem to appear. Is there a document that can be referred, or a tutorial that I can follow?

Thanks.

Dinuke

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

1) First, add the platform component

2) You have to click on the + button to add the compatible component

0693W000004KVJoQAO.png 

Best regards

Erwan

View solution in original post

3 REPLIES 3
Erwan YVIN
ST Employee

Hello Dinuke ,

There is a help section in SPC5Studio , (Cf Help Section)

you can add any compatible component, configure and generate the code.

Best Regards

Erwan

0693W000004KQZ3QAO.png 

Hello Erwan,

I followed the help section. I have already created a new SPC5Studion application. I cant unable to find compatible components. Where do I can find the compatible components.

Best Regards,

Dinuke

1) First, add the platform component

2) You have to click on the + button to add the compatible component

0693W000004KVJoQAO.png 

Best regards

Erwan